Michigan
Background
This automaker's corporate headquarters includes classrooms where employees who manufacture the vehicles can take classes to expand their knowledge, keep up with trends, and hone their skills.
For this project, the company wanted to upgrade the lighting in two adjacent classrooms.

Challenge
Each of the two classrooms could accommodate 40-50 people. The classrooms had two zones: a general classroom zone and a smaller front-of-the-classroom zone that included a whiteboard and/or a video screen.
The automaker wanted to upgrade the classroom lighting, keeping everything as simple and easy as possible.
Solution
The automaker chose to work with Superior Electric and Clarus Lighting + Controls, companies they trust for most of their lighting needs.
Having worked with Cooper Lighting Solutions for many years, Clarus Lighting + Controls knew that Metalux lighting and WaveLinx CAT wired controls from Cooper Lighting Solutions would be ideal for this project.
Metalux indoor lighting is an exceptional value that helps reduce costs and energy. All of the old classroom fixtures were replaced with Metalux AchievaTM Recessed Selectable troffers. In addition, two switchpacks were installed in each classroom to accommodate the two zones that were created. And WaveLinx CAT lighting controls were installed.
WaveLinx CAT controls were easy to commission. WaveLinx CAT wired controls are designed to be programmed and reprogrammed to make changes with ease – and without the need for an electrician.
Andy Meeter, principal at Clarus Lighting + Controls, explains just how simple WaveLinx CAT makes it for users to program the controls.
“The clients downloaded the app and created an account. Then I showed them how to use it. If they ever want to change a scene or something else, they’ll be able to do it themselves. It’s not hard at all.”
During the job, WaveLinx CAT lived up to its reputation for flexibility. Because an existing classroom door had to be relocated to another wall, WaveLinx made it a simple matter to move the corresponding switchpack, too, without the need for rewiring.


Our client required a quick and simple code compliant controls solution for their classrooms. WaveLinx CAT from Cooper fit the bill from arriving quickly, installing easily, and getting the classrooms operational in a very tight time frame.Kevin Kennedy, Senior Project Manager, Superior Electric Great Lakes Co.
Results
The car company as well as Superior Electric were very happy with the results of this project and particularly the advantages they enjoyed because of Cooper Lighting Solutions WaveLinx CAT controls.
Fast and Easy Installation WaveLinx CAT controls work out of the box.
No Engineers or Electricians Necessary Programming/commissioning the WaveLinx system is super easy via app and smartphone.
Flexible Reprogramming is easy, too. If the automaker were to change these rooms from classrooms to, say, conference rooms, it would be a simple matter to reprogram the system.
Future-Ready If the car company wanted to upgrade to a network solution, WaveLinx CAT integrates seamlessly with the Cooper Lighting Solutions WaveLinx wired system to create a hybrid lighting control system that combines the advantages of both wired and wireless solutions.
Optimized Light & Energy Savings WaveLinx CAT helps the company use less energy to light its classrooms and enjoy the related energy cost savings
Talk to a lighting controls professional.