Ephesus Sports Lighting Systems
Case Studies
Professional LED Stadium Lighting

Stadium Lighting
State Farm Stadium, NFL Football Stadium Lighting
State Farm Stadium, home to the Arizona Cardinals and host to the 2015 Super Bowl, installed 312 Ephesus Stadium Pro LED light fixtures. The Ephesus solution used a wired DMX control system that enabled instant control of light settings and levels as well as the ability to generate unique effects.

Stadium Lighting
Globe Life Park in Arlington, MLB Stadium
Home of the Texas Rangers, Globe Life Park sees a lot of action. For years, the field was plagued by varying light levels, and operators wanted the ability to create dynamic scenes and effects. We eliminated hundreds of fixtures while increasing illumination and uniformity.

Stadium Lighting
Nyseg Stadium, Milb Stadium
New ownership assumed operation of the team in late 2015 with the goal of turning things around, which included a desire to make the ballpark more fan-friendly. The facility underwent a $3.5M renovation before the 2017 season. In addition to the lighting, improvements included a new bullpen and batting cage, and more. Ephesus All Field retrofitted the existing stadium lighting, replacing the antiquated metal halide fixtures with 750 All Field Fixture.

Race Track Lighting
Martinsville Speedway, Nascar Track
Martinsville Speedway is an iconic 70-year-old motorsport track in Ridgeville, VA, that, up to now, never had permanent lighting. Any lit events required temporary lighting and generators, which provided poor lighting while being cumbersome and expensive. That's where Ephesus stepped in.
Collegiate / University

Stadium Lighting
Hoover Metropolitan Stadium
Ephesus' sports lighting was able to increase light levels by more than 50 percent to satisfy SEC Tournament broadcast standards and NCAA Tournament requirements which will open the venue up to potentially hosting NCAA Regional Championship games.

Stadium Lighting
Sanford Stadium at the University of Georgia, NCAA Div I Football Stadium Lighting
Sanford Stadium is the on-campus football venue at the University of Georgia in Athens, Georgia. The 92,746-seat stadium is the ninth-largest stadium in the NCAA. Georgia's average home attendance has ranked among the nation's top 10 for more than two decades. Surrounded by its famous hedges, Georgia's home field is one of the legendary facilities in college football.

Stadium Lighting
Virginia Tech Thompson Field | Soccer and Lacrosse Athletic Complex Project
Virginia Polytechnic Institute and State University's Thompson Field serves as the home of the men's and women's soccer teams as well as the lacrosse team. Expanded since it was opened in 2003, the venue now features approximately 2,028 seats with unobstructed views and the spacious area around the field allows for nearly 1,500 more fans to watch games.

Stadium Lighting
Superior Dome at Northern Michigan University, Collegiate Football Stadium Lighting
Northern Michigan University's Superior Dome is the home of the Northern Michigan University football team, marching band and a variety of other campus and community events. The dome, which opened in 1991 and has a seating capacity of 8,000, is the largest wooden dome in the world.

Stadium Lighting
Williams Field at Duke University, NCAA Field Hockey Pitch
Williams Field became the first NCAA Division I outdoor college sports venue to be lit with LED lighting. The Ephesus wireless control system was also used in this project to allow for enhanced fan experience as well as operational flexibility.

Track & Field Stadium Lighting
Wildcat Stadium at Abilene Christian University, NCAA Football Stadium Lighting
Anthony Field at Wildcat Stadium is home to Abilene Christian University football. The facility was newly-constructed and opened prior to the 2017 season, bringing football back to a permanent on-campus venue for the first time since 1942. Prior to construction, ACU shared a stadium with a neighboring high school and spectators had to drive or be bused off-campus for Wildcat home games. The new stadium accommodates 12,000 spectators.
Municipal / High School

Stadium Lighting
Reavis High School - Hanke Stadium
Using a combination of Ephesus' LED sports lighting and state-of-the-art digital lighting control solutions, the upgraded system provided Reavis High School with 60% less energy usage compared to a similar system using metal-halide technology.

Stadium Lighting
Pelcher Arcaro Stadium, High School Stadium
The school district wanted to reduce energy costs and maintenance associated with the existing sports lighting and upgrade the lighting quality in general. In addition to retrofitting the stadium, the Ephesus solution included wireless controls to increase operational flexibility as well as provide remote control and monitoring.

Football Stadium Lights
Sprayberry High School
Learn how Jim Frazier Stadium upgraded their metal-halide fixtures to Ephesus LumaSport 8 lights to reduce energy consumption by 62%.

Football Stadium Lights
Piedmont USD, High School Stadium
Witter Field at Piedmont High School is home to Piedmont's football, baseball, soccer, track & field, lacrosse, and softball teams. The facility is used by both the school and community sports teams seven days a week.

Football Stadium Lights
Juan Diego Catholic High School, Hs Stadium
Juan Diego Catholic High School was founded in 1999. Its stadium is heavily used, between games and practices for football, boys and girls lacrosse, soccer, cheer and other events. The Soaring Eagles football team has won five state championships in the last ten years, most recently in 2017.
Professional LED Arena Lighting

Arena Lighting
Bridgestone Arena, NHL Hockey Arena
This popular arena sought lighting upgrades to enable more sophisticated productions, save on energy and increase flexibility. It became the first arena to install a color temperature tuning LED lighting solution.

Arena Lighting
Canadian Tire Centre, NHL Hockey Arena
We installed 146 Ephesus Arena fixtures, in addition to wireless controls and the Ephesus Black Box control system. This provides instant, one-touch control to switch between different light settings as well as the ability to create unique fan experience effects. Custom lighting scenes were developed to the customer's specifications.

Arena Lighting
Herb Brooks Arena | Olympic/Multi-Event Project
Made famous during the 1980 Winter Olympics when the U.S. hockey team's 'Miracle on Ice' game beat Russia and named after the late Herb Brooks, the 7,700-seat multi-purpose arena hosts national and international figure skating competitions, NCAA men and women's hockey, USA Hockey events, Disney on Ice, annual ECAC Hockey Championships, trade shows and more.

Arena Lighting
Utica Memorial Auditorium, AHL Hockey Arena
The Utica Memorial Auditorium (The AUD) is home to the AHL's Utica Comets. Ephesus installed Arena sports lighting and Prism color fixtures as well as a wireless control system to provide the ultimate fan experience.

Arena Lighting
Bmo Harris Bank Center, AHL Hockey Arena
The AHL-affiliate Rockford Ice Hogs call the 10,000-seat BMO Harris Bank Center venue home, and with its new Ephesus LED lights and wireless control system, they have improved operational use and fan experience.
Collegiate / University

Arena Lighting
Watsco Center at University of Miami, NCAA Division I Basketball Arena
The Center selected the Ephesus Arena Pro for its color temperature tuning capability and controllability.

Arena Lighting
Liacouras Center at Temple University, NCAA Division I Basketball Arena
Ephesus Arena and Prism fixtures were installed at this Division I NCAA institution, generating an average of 155fc on the playing surface.

Arena Lighting
Convocation Center at Ohio University, NCAA Division I Basketball Arena
Ephesus was able to reduce Ohio University's fixture count from one hundred and fifty-five Metal Halide fixtures, to fifty-two Ephesus Arena 600 fixtures. The Ephesus fixtures were laser-focused to provide better light uniformity and consistency.

Fieldhouse Lighting
Nicholson Fieldhouse at UCF, NCAA Div I Football Venue
Nicholson Fieldhouse is the practice facility for University of Central Florida's Knights NCAA Division I football team, who were undefeated in their 2017 season. The fieldhouse was built in 2005 and was the first indoor practice facility at any of Florida's DI football programs.