- UL 8802 Safety Rated
- System ready and System On LED indicator lights
- Universal keyed activation switch
- Fits in standard double gang wallbox
CLS
UV-C User Station
Overview
The UV-C User Station allows a trained operator to control the UV-C System. There are 4 components of the User Station: an ON/OFF switch, an LED indicator notifying the user the pushbuttons and sensors are in the closed position, a keyed switch which only allows trained staff to operate the system and another LED light which indicates if the system is actively running.